Incucyte® Proliferation Assays for Live-Cell Analysis

What is Cell Proliferation?

Proliferation is an essential mechanism for normal tissue development, regeneration and renewal. Aberrations in cell proliferation, however, can give rise to malignant transformation and cancer pathology. Detecting changes in proliferation, as well as the ability of cells to divide in response to stimulus, is critical in oncology and stem cell research as well as drug testing for efficacy and safety.

Although there are multiple types of biochemical cell proliferation assays, challenges exist that limit a scalable method for robust quantification:

  • Tedious, manual sample preparation
  • End-point assays limiting measurements to a single time point
  • Inability to monitor effects of multiple treatments within the same cells
  • Limitations on treatments to be studied due to lack of throughput 
  • Most are indirect and subject to artifacts that cannot be readily verified by morphological changes.

The Incucyte® Live-Cell Analysis System alleviates these shortcomings by using multiple strategies to measure the same sample over time. Using either integrated, powerful software tools and artificial intelligence (AI), or combining this label-free approach with non-perturbing reagents, quantification of cell proliferation at a microplate level has never been easier.


Incucyte® live-cell analysis solutions include:

  • Non-invasive, image-based measurements of cell growth based on area (confluence) or cell number (count) metrics, visually verified via images and movies
  • Selection of label-free or fluorescent assays depending on the specific scientific question being asked and the cell models studied
  • Continuous live-cell assays for both adherent and non-adherent cells in which the cells remain stationary inside a standard tissue culture incubator while Incucyte® optics move
  • Cells within the same population are tracked continuously over time via repeated interrogation of the same well, without loss of environmental control
  • Real-time data can distinguish temporal differences in drug or treatment effects and enable decisions as experiments progress


Incucyte® Proliferation Assay Concept

  • Measure cell proliferation using live-cell time-lapse imaging, with or without labels, using Classic Confluence Analysis or new AI Confluence Analysis
  • Easily generate long-term growth and growth-inhibition curves and monitor morphology
  • Directly measure changes in true cell number (nuclear count) over time using Incucyte® Nuclight Reagents for live-cell labeling. Automatically analyze growth curves and extrapolate doubling times
  • Explore co-cultures using green, red, orange or NIR Incucyte® Nuclight Lentivirus Reagents
  • Multiplex proliferation readouts with measurements of apoptosis or cytotoxicity by combining with the Incucyte® Caspase-3/7, Incucyte® Annexin V  or Incucyte® Cytotox Dyes

   

Request More Information
   
See All Applications


eBook

Live-Cell Analysis Handbook: 6th Edition

Discover how the power of artificial intelligence for label-free, live-cell imaging and analysis is moving research forward and driving deeper discove...

Incucyte® Proliferation Assays

Introducing Incucyte® Proliferation Assays

The Incucyte® Live-Cell Analysis System enables real-time, automated quantification of cell proliferation assays inside your tissue culture incubator:

(1) Label-free, Confluence

Confluence can now be measured in two different ways - both included in the Incucyte® Base Analysis Software. The first method, Classic Confluence, is the existing segmentation algorithm that allows the user to tailor phase segmentation parameters to individual cell types and experimental conditions. The second segmentation method, the new AI Confluence algorithm, is a robust, AI-driven analysis designed to adapt to a wide range of cell types and morphologies while requiring less user input. 

Monitor proliferation of SKOV3 cells in real time with confluence image mask (Yellow) using Incucyte® Base Analysis Software with AI Confluence segmentation.

(2) Label-free, Direct Cell Count

Using the Incucyte® Cell-by-Cell Analysis Software Module, cell proliferation can be quantified by counting the number of phase objects over time. By identifying individual cells, a label free count can be achieved until the point that cultures become densely packed. In addition, subsequent classification of cells into subpopulations can be performed based on properties such as size, shape and fluorescence intensity.

The Incucyte® Advanced Label-Free Classification Analysis Software Module is available as an add-on that allows objective tracking of adherent cell populations kinetically. 

Monitor proliferation of NALM6 cells in real time with Incucyte® Cell-by-Cell Analysis Software Module (mask shown in yellow).

(3) Fluorescent Labeling, Direct Cell Count

Cell proliferation is quantified by counting the number of fluorescent nuclei over time to give true cell growth rates. Cells are labeled with nuclear-restricted non-perturbing fluorescent labels (e.g., Incucyte® Nuclight Green Lentivirus). In co-culture, different labels can be combined to simultaneously measure proliferation of up to three cell types.

Monitor proliferation of HT-1080 cells stably expressing Incucyte® Nuclight Green, Nuclight Orange or Nuclight NIR Lentivirus in real time using Incucyte® Cell-by-Cell Analysis Software Module.

Key Advantages of Incucyte® Proliferation Assays

Request More Info 

View Incucyte® Proliferation Publications

Identify and Segment Cells Label-Free, Using AI-driven algorithms to Measure Confluence

Quantify changes in proliferation using label-free, intuitive software analysis.

The Incucyte® Base Analysis Software includes two different tools to measure confluence: the AI Confluence Analysis, and the Classic Confluence Analysis. Fluorescence image acquisition and analysis of Cell Health or Viability assays are also available with Incucyte® Base Analysis Software, Classic Confluence Analysis definitions.

The AI Confluence Analysis is driven by a neural network trained on many classes of cells, which provides a simple, objective, and repeatable workflow with minimal user input for highly accurate segmentation of cells in phase contrast images. 

The Classic Confluence Analysis enables users to refine phase segmentation parameters to individual cell types and experimental conditions to accurately distinguish between background.

Figure 1: Analyze label-free confluence with integrated software tools. AI-driven confluence analysis offers efficient, objective analysis (A workflow). Classic Confluence Analysis utilizes incorporates user-defined segmentation based on experimental conditions (B workflow). 


Figure 2. Robust segmentation of cell confluence using AI Confluence Analysis. A549, MDA-MB-231, SKOV3 and HT-1080 cells were seeded into a 96-well plate at a range of densities (0.5 – 10K cells/well). High definition (HD) phase-contrast images were acquired every 2h and cell proliferation was measured over 4 days. Yellow outline indicates AI Confluence segmentation and plate view reports % Confluence over 4 days.


Conduct Cell Counting/ Proliferation for High-Throughput Compound Testing

Real-time measurements of cell health and proliferation are essential for studying the effects of drugs, culture conditions or genetic modifications on cell growth or viability. Identify individual cells and generate label-free, true cell counting, in both non-adherent or adherent cell modules, with the Morphological Analysis in the Incucyte® Cell-by-Cell Analysis Software Module.

Figure 3 : Label-free cell counting in adherent and non-adherent cell types using Incucyte® Cell-by-Cell Analysis Software Module. Various densities of adherent Incucyte®  Nuclight Red A549 or non-adherent Incucyte® Nuclight Red Jurkat cells were analyzed over time with Incucyte® Cell-by-Cell Analysis Software Module.  Red Object Count was used to validate the Incucyte®’s label-free cell counting method. Images demonstrate individual cell masking using the Cell-by-Cell Analysis. Time course of Phase Count and Nuclight Red Count across densities shows overlay of label-free and fluorescent data. This validation has been repeated across a range of cell types (date not shown). Values shown are mean ± SEM for 4 wells.

Table 1. Drugs identified in literature as relevant to cell proliferation. To assess many pharmacological agents simultaneously, 16 literature-standard compounds (Table 1) were applied to HT-1080 cells in a 384-well format.

Figure 4. 384-well microplate view of Incucyte® Nuclight Green HT-1080 cell proliferation in response to treatment. Incucyte® Nuclight Green HT-1080 cells were treated with16 different compounds, 11-point concentration-response curves in duplicate (different colors, high to low concentrations left to right). Columns 15 and 16 are vehicle (0.5% DMSO) and CHX (3 μM) controls, respectively. Note the potent concentration-dependent inhibition of cell proliferation for certain compounds (e.g., Row J, Row M, Row O), and weaker effects/inactivity of others (e.g., Row A, Row P). Abscissa: Time (0-72 hours), ordinate: Fluorescent Object Count per well (0-3800).


Quantify Proliferation and Multiplex with other Cell Health Dyes

Combine Incucyte® Proliferation Assays with Incucyte® Cytotox, Incucyte® Annexin V or Incucyte® Caspase 3/7 Dyes for multiplexed measurements of cytotoxicity/ apoptosis. Readily discriminate between cytotoxic and cytostatic treatment effects

Confirmation of apoptotic cell death with two readouts (Caspase-3/7 and Annexin V) on the Incucyte® live-cell analysis system. Note: data is shown as example and is not related to studies mentioned in this interview.

Figure 5: Detect both Caspase 3/7 and Annexin V signals in cultures. Automatically determine the time courses of apoptotic cell death and correlate with label-free confluence measurements to provide an estimate of the proportion of apoptotic cells within the population (apoptotic index).

Ordering Information

Technical Resources

Literature and Documentation

Article

AI-Powered Software Tools

Enable Automated and Unbiased Live-Cell Health Analysis

AI Confluence Analysis 1-Sheet

Reagents and Consumables Brochure

Kinetic Quantification of Cell Proliferation Using Live-Cell Analysis

Incucyte® Cell Proliferation Assay Protocol

Incucyte® Nuclight Lentivirus Reagents Product Guide

Incucyte® Nuclight Lentivirus Reagents enable efficient, non-perturbing, nuclear labeling of living mammalian cells.

Incucyte® Cell Cycle Lentivirus Reagents Product Guide

Continuous live-cell proliferation, clustering and viability assays fo...

Multiplexed Incucyte® Cell Health & Phenotypic Assay

white paper thumbnail
White Paper

Label-Free Imaging and Kinetic Analysis in Live Cells

Developments in advanced software tools for label-free analysis, including our first software module to use a neural network

Related Applications

apoptosis

Apoptosis

Cytotoxicity

Cell-by-Cell Analysis

Morphological Analysis

icon-file-text

14,000+ Incucyte® Publications

Incucyte® helps explore new areas of study and address questions about life science research.

Explore Publications

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request a Demo, Literature, or More Information